DOCA0270EN-03

Alarms – Corrective Actions

Alarms inform you of potential issues with the island. They do not affect the avatar or the state of the island. The following are potential internal events and protection alarms you might encounter during operation.

NOTE: Use the Event Log to help determine the cause of alarms on the system.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?