DOCA0270EN-03

Rapid Cycle Lockout

The Rapid Cycle Lockout function helps prevent potential harm to the motor caused by repetitive, successive inrush currents resulting from too little time between starts.

If this protection function is enabled, the TeSys avatar ignores Run commands for the duration specified by the Rapid Cycle Lockout Timeout, starting from the last transition to the motor Start state.

No alarm or trip is associated with this function.

Rapid Cycle Lockout Timeout

Ir

Rated Current

A

Rapid Cycle Lockout Timeout

B

New Run Commands Ignored

C

New Run Commands Not Ignored

D

Transition into Motor Start State

t

Time

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?