DOCA0270EN-03

Alarm and Trip Counters

Protection functions increment alarm and trip event counters, both at the TeSys avatar level and overall at the TeSys island level. Counters can be reset to zero on demand.

The following tables describe counter behavior.

Counter Inputs

Inputs

Description

Alarm Counter Reset

Resets all alarm counters (see the following table) to zero.

Trip Counter Reset

Resets all trip counters (see the following table) to zero. All avatars store the last five trip records, each containing the timestamp and cause of the trip.

List of Alarm Counters

Outputs

Description

Thermal Overload Alarm Count

Increments when an individual alarm is triggered. Reset by Alarm Counter Reset

Jam Alarm Count

Undercurrent Alarm Count

Overcurrent Alarm Count

Current Phase Unbalance Alarm Count

Ground Current Alarm Count

All Alarms Count

Increments when any type of protection alarm is triggered. Reset by Alarm Counter Reset.

List of Trip Counters

Outputs

Description

Thermal Overload Trip Count

Increments when an individual trip is triggered. Reset by Trip Counter Reset

Jam Trip Count

Undercurrent Trip Count

Long Start Trip Count

Overcurrent Trip Count

Stall Trip Count

Current Phase Unbalance Trip Count

Phase Configuration Trip Count

Ground Current Detection Trip Count

Current Phase Reversal Trip Count

Current Phase Loss Trip Count

All Trips Count

Increments when any type of protection trip is triggered. Reset by Trip Counter Reset.

Records of the Last Five Trips

Outputs

Description

Trip Record Register 1 (most recent)

First In First Out registers without reset

Trip Record Register 2

Trip Record Register 3

Trip Record Register 4

Trip Record Register 5 (least recent)

List of Auto-Reset Counters

Outputs

Description

Thermal Protection
Auto-Reset Retry Count

Provides the number of auto-reset retry attempts for Thermal Protection functions. If there is no trip within one minute after a retry attempt, the start is considered successful and Auto Reset Retry Count is reset to 0.

Electrical Protection
Auto-Reset Retry Count

Provides the number of auto-reset retry attempts for Electrical Protection functions. If there is no trip within one minute after a retry attempt, the start is considered successful and Auto Reset Retry Count is reset to 0.

Load Protection
Auto-Reset Retry Count

Provides the number of auto-reset retry attempts for Load Protection functions. If there is no trip within one minute after a retry attempt, the start is considered successful and Auto Reset Retry Count is reset to 0.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?