DOCA0270EN-03

Recovering from Degraded Mode

You can enable the Degraded mode auto-reset option in the TeSys island DTM Library. If Enable Degraded Mode Auto-Reset is set to Yes, then TeSys island exits Degraded mode when communication is restored.

If the option Enable Degraded Mode Auto-Reset is set to No, then a system restart command or power cycle is required to exit Degraded mode.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?