DOCA0270EN-03

Bus Coupler

If you click the bus coupler in the island view, a new window displays the status of the bus coupler. The following information is provided for the bus coupler:

  • Device Status

    • Name tag

    • Position

    • Commercial reference number

    • Status

    • Irms

    • Upstream voltage presence

  • Asset Data

    • Number of device power cycles

    • Time device on

    • Number of events

  • Product Identification

    • Vendor name

    • Vendor URL

    • Produce name

    • MAC address

    • Serial number

    • Vendor ID

    • Firmware version

    • Product code

  • Device Logs

  • Locate Command

Island View: Bus Coupler

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?