DOCA0270EN-03

Thermal Overload

The Thermal Overload protection function is based on a thermal model which calculates the used thermal capacity of the motor.

If enabled, this function performs the following:

  • Signals a Thermal Overload Alarm when the motor thermal capacity used exceeds the Overload Alarm Level

  • Triggers a Thermal Overload Trip when the motor thermal capacity used exceeds 100%

The Thermal Reset Threshold parameter sets the percentage below which the motor thermal capacity used must fall, before a thermal overload trip reset is allowed.

NOTE: For single phase, thermal overload protection uses only I1 and I3.

Thermal Overload Protection Trip and Alarm

I1

Phase 1 Current

I2

Phase 2 Current

I3

Phase 3 Current

A

Motor Thermal Model

B

Motor Thermal Capacity Used ≥ 100%

C

Motor Thermal Capacity Used ≥ Thermal Overload Alarm Level

D

Thermal Overload Trip

E

Thermal Overload Alarm

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?