DOCA0270EN-03

Loading the Project File to the Island

SoMove software with TeSys island DTM allows you to import a project file created with the Motor Control Configuration tool. Or you can use SoMove software to build a new TeSys island and generate the project file without being connected to the TeSys island.

After you have created the project file and powered up the island, you can connect the PC running SoMove software to the service port on the bus coupler, or you can connect a Wifer to the service port and communicate using Wi-Fi. The TeSys island DTM has a built-in scan mechanism that discovers the available TeSys island on the network. Once the scan is complete, you can use the Locate command in the tool to trigger a visual LED indicator on the bus coupler of the correct TeSys island. Once you are connected to the TeSys island, use SoMove software to load the project file for the TeSys island to the bus coupler.

Perform the steps in the table below to load the project file.

Load the Project File to the Island

Step

Action

1

Launch SoMove software.

2

Connect to the TeSys island.

3

Click Store to Device.

4

Select the project file that you wish to load to the bus coupler from the PC.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?