DOCA0270EN-03

Exit Test Mode

Once you complete the Test mode activities, you must manually exit Test mode to return the island to the operational state:

  1. Click the Diagnostics View panel.

  2. Click the Exit Test Mode button.

    Exit Test Mode

  3. A pop-up appears. To confirm that you want to exit Test mode, click OK.

    NOTE: The status banner at the top does not indicate that the system is no longer in Test mode.

    Exit Test Mode Confirmation

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?