DOCA0270EN-03

Powering Up the Island

To power up TeSys island, perform the steps in the following table.

Powering Up the Island

Step

Action

1

Energize the bus coupler with 24 Vdc. The island will enter a pre-operational stage once it has completed booting.

2

Check the visual indicators on the bus coupler. See TPRBCEIP – Bus Coupler LEDs

  • The PWR LED on the bus coupler, which indicates power supply and system status, should be steady green.

  • TPRBCEIP — The MS LED, which indicates bus coupler status, should be flashing green, indicating that the island has not yet been configured.

  • TPRBCPFN — The BF LED, which indicates an inoperative bus coupler system, should be red, indicating that the island has not yet been configured.

  • TPRBCPFB — The COM LED, which indicates bus coupler status, should be flashing red acyclic (two quick flashes per second), indicating that the island has not yet been configured.

TPRBCEIP – Bus Coupler LEDs

TPRBCPFN – Bus Coupler LEDs

TPRBCPFB – Bus Coupler LEDs

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?