DOCA0270EN-03

Analog I/O Module

The main functions of the analog I/O module are as follows:

  • Monitor voltage or current from analog sensors (such as thermocouple, PT100, PT1000, NI100, NI1000, PTC Binary) via two −10 to +10 V /

    0 to 20 mA
    capable inputs

  • Control voltage-driven actuators (such as variable speed drives or a current loop to the controller’s analog input) via one −10 to +10 V / 0 to 20 mA capable output

  • Capture statistical operational data:

    • Number of power cycles

    • Number of device events

    • Time the module is on

The reference number is TPRAN2X1.

The analog I/O module is connected:

  • Upstream to the 24 Vdc source needed to power the downstream actuators

  • Input channel: downstream to an analog sensor or sensor transmitter

  • Output channel: downstream to the control input of a voltage-driven actuator, such as a variable speed drive

Refer to Avatar Wiring Schematics for module wiring.

Devices connected to the analog I/O module must be protected against short circuits by external means like fuses.

The analog I/O module communicates with the bus coupler, sending operational data and receiving commands.

NOTE: No per-channel LEDs are provided.

Input/Output Specifications

Channel

Inputs

Output

Number of analog inputs and outputs

2 isolated with common point

1 isolated

Rated power supply

24 Vdc

Resolution, maximum

16 bits, or 15 bits + sign

12 bits (4096 points)

Cable type

Twisted pair shielded

Cable length, maximum

30 m (98 ft)

Signal Type: Inputs

Channel

Inputs

Signal type

Voltage (Vdc)

Current (mA)

Thermocouple

3–wire RTD (Resistance Temperature Detector)

Range

  • 0 to 10

  • −10 to +10

  • 0–20

  • 4–20

  • Type K, J, R, S, B, E, T, N, C

  • PTC Binary

PT100, PT1000, NI100, NI1000

Signal Type: Outputs

Channel

Output

Signal type

Voltage

Current

Range

  • 0 to 10 Vdc

  • −10 to +10 Vdc

  • 0–20 mA

  • 4–20 mA

Analog I/O Module Features

Flat cable (for connection with the module to the left)

QR code

LED status indicators

Name tag

Connector with spring terminals

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?