DOCA0270EN-03

Reset System

After a minor event occurs, execute this command to reset the system.

  1. Click the Control Panel icon.

  2. Click Reset System.

    Result: The island resets.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?