DOCA0270EN-03

Motor Two Directions - SIL Stop, W. Cat 1/2

NOTE: Safety Integrity Level according to standard IEC 61508. Wiring Category 1 and Category 2 according to ISO 13849.

Wiring (See Legend Table below.)

Accessories

Legend

A

Mechanical interlock

B

Parallel link

C

Reversing link

F

Forward

R

Reverse

SS-1

SIL starter 1

SS-2

SIL starter 2

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?