DOCA0270EN-03

SIL Stop Events

NOTE: Safety Integrity Level according to standard IEC 61508.

TeSys island logs the following SIL Group Stop events for SIL groups 1–10:

  • Not yet in SIL Stop State

  • SIL Stop State achieved

  • Wiring issue, in SIL Stop State

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?