DOCA0270EN-03

Minor Events – Corrective Actions

When the TeSys island encounters a minor event:

  • The fieldbus and service ports remain activated.

  • Only the System or Avatar is activated.

  • All power modules and I/O modules are in the device Off state.

  • To exit a minor event state that is not automatically recovered, a system reset, restart, or control power cycle is required. A system reset command can be issued manually from the TeSys island DTM, the OMT, or the PLC.

    @New in Draft1 V03
    NOTE:
    • During a minor event at system level, the whole island system will be de-energized.

    • During a minor event at avatar level, only the respective avatar will de-energize instead of the whole system.

The following scenarios cause the island to encounter a minor event:

Minor Events and Corrective Actions

Minor Event

Diagnosis

Corrective Action

Topology mismatch

The island configuration in the active context file does not match the actual discovered topology of the island

Determine the proper configuration and align the configuration with the physical hardware

The OMT and the DTM have a compare function in the diagnostics views to compare the topology.

Perform one of the following:

  • System Reset

  • System Restart

  • Control power cycle

Switch off island command

Island received Switch Off Island command

N/A

Too many modules

The number of physical modules detected in the island is beyond the maximum allowed limit of 21

  1. Power down

  2. Remove modules to meet the 21 maximum requirement

  3. Power on

No modules on island

There are no physical modules installed on the island

Complete the installation of the modules on the island

Control voltage 120%

The voltage was over 120% for longer than the allowed duration

Verify that the power supply voltage is within range

Firmware update unsuccessful

Firmware download to the device was unsuccessful after three consecutive tries

  • Check for the latest version of firmware available

  • Contact support

Summary file integrity check

Configuration file corruption detected

  • Download a new configuration file to the island

  • Verify that the micro SD card is functioning properly

Context file integrity check

Configuration file corruption detected

  • Download a new configuration file to the island

  • Verify that the micro SD card is functioning properly

Avatar settings file integrity check

Configuration file corruption detected

  • Download a new configuration file to the island

  • Verify that the micro SD card is functioning properly

Avatar settings file malformed

Configuration file corruption detected

  • Download a new configuration file to the island

  • Verify that the micro SD card is functioning properly

No active project file

Bus Coupler is not configured with an active project file

Configure Bus Coupler using engineering tools

Range of voltage supply

Confirm the sufficient voltage supply

In order to run the TeSys island, the voltage supply must be higher than 20.7 V.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?