DOCA0270EN-03

Process Variables

Application and load avatars introduce Process Variable (PV) inputs and switches:

  • PV inputs receive analog values from sensors such as pressure meters, flow meters, or vibration meters. PV inputs connect to analog I/O modules (AIOMs) that are included as part of the avatar. The number of AIOMs required for the avatar is determined based on the number of configured PV inputs.

  • PV switches receive discrete signals from switches such as float switches or proximity switches. PV switches connect to digital I/O modules (DIOMs) that are included as part of the avatar. The number of DIOMs required for the avatar is determined based on the number of configured PV switches.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?