DOCA0270EN-03

Island Topology Change Events

TeSys island logs the following Island Topology Change events in the Audit Log:

  • Device added

    The bus coupler has discovered a new device that has not been addressed. This event is detected when the bus coupler receives any response to a “Read Device ID Out” message, periodically sent to Bus Device address 127, requesting Device ID information.

  • Device removed

    The bus coupler has detected that a Bus Device has stopped communicating on the bus.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?