DOCA0270EN-03

Coupling Starters

This section describes how to join adjacent starters with accessories for use in two direction, two speed, and wye-delta Avatars. Refer to the bill of materials (BOM) and the TeSys island topology to determine which starters require installation of accessories. See also Avatar Composition. Join the starters with the accessories before mounting them on DIN rail.

The accessories come packaged as kits or can be ordered individually. The kits and their components are described in the following tables.

LAD9R1 Assembly Kit for 9–38 A (Size 1 and 2) Starters

Kit Components

Description

LAD9R1 Assembly Kit

LAD9V5

Parallel link between two starters

For installation instructions, refer to Installing the LAD9R1 Kit (9–38 A Starters).

LAD9V6

Reversing link between two starters

LAD9V2

Mechanical interlock with assembly staple

LAD9R3 Assembly Kit for 40–65 A (Size 3) Starters

Kit Components

Description

LAD9R3 Assembly Kit

LA9D65A6

Parallel link between two starters

For installation instructions, refer to Installing the LAD9R3 Kit (40–65 A Starters).

LA9D65A69

Reversing link between two starters

LAD4CM

Mechanical interlock

Shorting Blocks for Y/D Avatars

Reference Number

Description

Shorting Blocks

LAD9P3

Shorting block / 3P parallel link for 9–38 A (size 1 and 2) starters.
Used for linking 3 poles of a contactor in a wye-delta (Y/D) starter.

For installation instructions, refer to Installing the LAD9P3 Shorting Block (9–38 A Starters in Y/D Avatars).

LAD9SD3S

Shorting block / 3P parallel link for 40–65 A (size 3) starters and a separate warning label.
Used for linking 3 poles of a contactor in a wye-delta (Y/D) starter.

For installation instructions, refer to Installing the LAD9SD3S Shorting Block (40–65 A Starters in Y/D Avatars).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?