DOCA0270EN-03

TeSys island Configurator

The TeSys island Configurator is an online tool accessible from the Schneider Electric website. The configurator is an intelligent catalog, computing and providing the island’s configuration based on the requirements entered for the specific application.

The TeSys island Configurator’s main purpose is as follows:

  • Capture the functional requirements of the application, and the electrical characteristics of the island

  • Compute the list of required TeSys island devices automatically

  • Generate the physical topology of the island

  • Generate the associated bill of materials

  • Generate the configuration files, which can be downloaded for re-use by EcoStruxure Machine Expert and SoMove software.

  • Provide access to technical documentation related to electrical panel engineering and automation control programming

The TeSys island Configurator can be found at www.se.com/en/work/products/industrial-automation-control/tools/motor-control-configurator.jsp.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?