DOCA0270EN-03

Current Phase Unbalance

The Current Phase Unbalance function only applies to three-phase TeSys avatars.

If enabled, this protection function performs the following:

  • Signals a Current Phase Unbalance Alarm when the current phase unbalance exceeds the specified Current Phase Unbalance Alarm Level

  • Triggers a Current Phase Unbalance Trip when the current phase unbalance exceeds the specified Current Phase Unbalance Trip Level for a time longer than the specified Current Phase Unbalance Trip Delay

    NOTE: Separate trip delays are configurable for Run State and Start State.

Current Phase Unbalance Trip and Alarm

I1

Phase 1 Current

I2

Phase 2 Current

I3

Phase 3 Current

%Iunb

%Current Phase Unbalance

Ialarm

Current Phase Unbalance Alarm Level

Itrip

Current Phase Unbalance Trip Level

T1

Current Phase Unbalance Trip Delay—Start

T2

Current Phase Unbalance Trip Delay—Run

A

Motor Start State

B

Motor Run State

C

Current Phase Unbalance Alarm

D

Current Phase Unbalance Trip

NOTE: The %Current Phase Unbalance value is
  • The maximum difference between any individual phase RMS current (in absolute value) and the average of the three-phase RMS currents

  • Divided by the average of the three-phase RMS currents

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?