DOCA0270EN-03

Certificate Manager

Certificate Manager allows you to configure security certificate to the TeSys island.

The user-supplied certificates can be only deleted. Once the certificate is deleted, the TeSys island assigns the self-signed certificate by default.

Self-signed certificate cannot be deleted and it can only be overridden by the user-supplied certificate.

To upload the certificate, do the following:

  1. In the Admin Options panel, click the arrow to expand the Certificate Manager.

  2. In the Upload Certificate window, click Choose File to select the .p12 certificate.

  3. Enter the certificate password and click Submit.

NOTE:
  • For certificate without password, leave the password field empty.

  • To support secure communications with HTTPS, the certificate must be imported in the browser of the PC.

Certificate Manager

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?