DOCA0270EN-03

Installation

This section summarizes the installation steps described in this guide. Turn off power before performing Steps 1–4. Read and understand the information in Precautions before performing any procedures in this guide.

1.

Receive and inspect the modules.

  • Check that the catalog numbers printed on the labels are the same as those on the purchase order.

  • Remove the modules from the packaging and check that they have not been damaged in shipping.

2.

Verify the supply mains.

Verify that the supply mains is compatible with the power supply range of the TeSys island.

3.

Assemble the TeSys island.

  • Assemble the TeSys island following the instructions in this guide.

  • Install any external options.

4.

Wire the TeSys island.

  • Connect the motor, ensuring that its connections correspond to the voltage.

  • Make sure that the power is off, then connect the supply mains.

  • Connect the control wiring.

5.

Set up the TeSys island.

6.

For operation, refer section OMT Operations.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?