DOCA0270EN-03

Conveyor One Direction - SIL Stop, W. Cat 1/2

Safety Integrity Level according to standard IEC 61508. Wiring Category 1 and Category 2 according to ISO 13849.

Wiring

NOTE: Analog I/O modules (AIOMs) and digital I/O modules (DIOMs) are configurable.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?