DOCA0270EN-03

Motor Two Speeds with Dahlandar Option

Wiring (See Legend Table below.)

Accessories

Legend

A

Mechanical interlock

D

Shorting block

LS

Low speed

HS

High speed

ST-1

Starter 1

ST-2

Starter 2

ST-3

Starter 3

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?