DOCA0270EN-03

Energy Monitoring

The Energy Monitoring functions provide several voltage, power, and energy measurements, both at the TeSys avatar level and for the full TeSys island.

These functions can be activated through the avatars Load Energy Monitoring setting, and require one voltage interface module to be installed in the island.

Energy is measured within a 10% accuracy for loads running under nominal conditions (50–125% FLA, power factor 0.7, 47–63 Hz).

NOTE: Active energy is measured, only when Current Phase Sequence is configured as ABC.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?