DOCA0270EN-03

Configuration Tools

TeSys island can be set up using the Operation and Maintenance Tool (OMT) and the latest TeSys island DTM.

The initial project file for the TeSys island can be generated using the TeSys island Configurator tool. This project file must be imported into the TeSys island DTM. It includes the TeSys island topology and the TeSys Avatars selected for the TeSys island. If the project file has not yet been created, SoMove software can be used to create the TeSys island project file in offline mode.

Once the configuration of the TeSys island and parameter selection is complete, SoMove software can be used to load the project file onto the bus coupler, which manages the settings of the entire TeSys island.

Once the TeSys island has been initialized, using the digital tools you can enter Test mode to verify that the power devices are functioning properly before applying the mains power supply and using Force mode to test the avatar logic.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?