DOCA0270EN-03

Voltage Interface Module (VIM)

Device Status is the top LED on all TeSys island modules except the bus coupler.

Device Status LED

Indicator State

Summary

Description

Single Flash Green/Red

LED Diagnostic

Visual indication that LEDs are operational.

Steady Off

Off

Module not energized.

Steady Red

Device Major Event

Internal device event.

Flashing Red

Not Ready

Discovery, addressing, firmware update, Device Minor Event, etc.

Steady Green

Ready

Module is ready.

Voltage Status is the second LED on the VIM.

Voltage Status LED

Indicator State

Summary

Description

Single Flash Green/Red

LED Diagnostic

Visual indication that LEDs are operational.

Steady Off

Off

Module not energized or not ready.

Flashing Green

Ready, No Voltage

Ready with no voltage detected.

Steady Green

Ready, Voltage

Ready with voltage detected.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?