Archive Services

Archive Services works much like Data Services. It provides the connection between Responder Archiver and the Responder archive tables in the geodatabase. Use the Archive Services tab to configure, manage and execute Archive Services. At least one Archive Services must be running in order to use the console (i.e., the Count field must contain a value greater than 0). At least one Archive Services must running to access Responder's Archive Explorer.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.