RX_SW_OR_FEATURES_ARCHIVE

Field Name

Description

SW_OR_FEATURES_ID

The ID associated with the switching order feature.

INCIDENT_ID

The ID associated with the incident resulting from the call. This field corresponds with the ID field in the RX_INCIDENTS table.

OID

Object ID of the feature associated with the tag.

FCID

Feature class ID of the feature associated with the tag.

SUBID

The unique ID of each segment of a complex edge.

X

The x-coordinate of the incident device.

Y

The y-coordinate of the incident device.

USER_CREATED

The name of the user who created the record. This field is populated automatically by Responder.

USER_UPDATED

The name of the user who updated the record. This field is populated automatically by Responder.

FACILITY_ID

The Facility ID of the incident device as defined in the geodatabase.

REGION

The region in which the feature exists. This field uses the REGION domain.

SUBSTATION

The substation that feeds the incident device.

COMMENTS

Notes from the operator or dispatcher.

ENABLED

Not used.

SUBTYPE

The subtype of the device.

FEEDER_ID

The Feeder ID of the feature.

PHASE_DESIGNATION

The phase designation of the device.

OPERATING_VOLTAGE

The operating voltage of the device.

NAME

The name assigned to the device.

CHANGE_DATE

The time and date an operation was performed on the record.

OPERATION

The operation (e.g., insert, delete, update) performed on the record.

USER_UPDATED_ARCH

This field is not currently used by Responder. You may customize Responder to populate this field with the name of the user who updated the record.

SW_ORDER_REQUEST_ID

The unique ID assigned to the switching order request.

AFFECTS_ENERGIZATION

Indicates whether the feature participates in the geometric network (electric device) or not (location feature).

FEATURE_CLASS_NAME

The name of the Feature Class on which the incident occurred, as it was configured/named when the Incident was archived.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.