Troubleshooting: "ORA-12154: TNS: could not resolve service name" error when running diagnostics on Responder Data Services

Problem: When using an Oracle database you must set up Local Service Naming for the database instance to which you are connecting. This error indicates that this instance is missing or incorrect.

Fix: Refer to the Configuring Responder topic for more information.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.