Change Context Position in Step Name

By default, when typing Context information for a Switching Order/Restoration Order step, the information appears at the beginning of the step name. Follow the steps below to change where in the step name the context appears:

TIP: As a reminder, if information is contained in the Context field, Context continues to appear in the step name even if the Show Context Information option is not selected from the View menu.
  1. Open Miner.Responder.Model.Switching.Properties.Resource.resx. By default, this file is installed here: C:\Program Files (x86)\Miner and Miner\ArcFM Solution\Resources\Responder.
  2. Look for any type of step name to modify, such as CloseDeviceTitle and locate the variable:

    {0:Context}

  3. Be default, the variable appears at the beginning of the title. You can move that variable to any position within the title.
  4. In addition, you can search for the version of the step name that also includes the device, such as CloseDeviceWithFormatTitle and change the position of the {0:Context} to any position within the title.
  5. Save and close Miner.Responder.Model.Switching.Properties.Resource.resx.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.