Permit Multiple Sessions Per Browser

This optional configuration allows you to host multiple sessions of Responder Web Portal in the same browser, on different tabs.

  1. Browse to the web.config file at this location: C:\Inetpub\wwwroot\Responder.
  2. Open Web.config. You can edit the file by opening it in an XML application (such as XML Spy) or by opening it in a simple text editing program (such as Notepad).
  3. Insert the following code in the <system.web> section, if not already added:
    <sessionState cookieless="true" regenerateExpiredSessionId="true" />
  4. Save and close Web.config. Restart the browser window.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.