Welcome and FAQs

Welcome to the Responder Configuration Guide.

Here are some tips to help you find relevant information fast:

  • Topics are organized thematically in the Table of Contents along the left-hand side. Expand topics to reveal subtopics.

  • Use the Search field to type keywords you’re looking for. The Search defaults to querying within the current guide, but it also gives you the chance to query the entire catalog of guides. Further, it allows you to filter by product, guide type, and version. Enter your search terms to get started.

    Watch this short video that walks you through how to perform a search and filter your results.

  • While reading a topic, press the down key to scroll down through the topic, press the right key to move to the next topic in the Table of Contents, and press the left key to move to the previous topic in the Table of Contents.

  • Want to send a topic to a co-worker? Click the Sharable Link tool. This copies the current topic’s URL straight to your clipboard, ready for you to paste into an email or other message.

    Want to see how the Shareable Link tool works in action? Watch this short video!

  • Is the image a little too small? Click it to open in a separate tab. It opens as large as possible.

  • Use the “Was this helpful?” feedback options to drop us a note! Your comments help us improve documentation so you can get your job done most effectively. The following video explains how the “Was this helpful?” button works.

  • Watch this video to learn more about navigating the ArcFM Solution Documentation Portal.


Frequently Asked Questions (FAQ)

What’s the user community searching for? Here are the top searches and topics visited in this guide:

Rx Config
  1. Do I need to have the same version of Responder installed as I have for ArcFM Desktop?

    1. Yes, you must be running the same version of Responder as you are ArcFM Desktop. Mixed versions are not supported.

  2. I'm using Oracle 18 or later, Responder doesn't start for me and displays "TNS:could not resolve the connect identifier specified." What do I need to do to fix this?

    1. Responder was updated in 10.6.1a to use Oracle Managed Driver to connect to Oracle databases. After creating the tnsnames.ora file, the Managed driver needs to know where the file is located. Access System Properties, then add the Variable Name TNS_ADMIN as an environment variable.

      Set the Variable value to the path where the tnsnames.ora file resides. For example: C:\app\client\username\product\18.0.0\client_1\network\admin

      You must also install ArcGIS (Desktop, Engine, Server) 10.6.1 Support for Oracle 18c Patch.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.