Enhanced Refresh

Enhanced Refresh uses a dataset merging algorithm leveraged from PubSub technology to provide a faster Full Refresh experience. We recommend all of our users enable this.

Users are still allowed the option to continue to use the legacy Full Refresh, if they are already comfortable with the function and performance of the tool.

To configure Enhanced Refresh add the following Miner.Responder.Explorer.config AppSetting if it is not already present:

<add key="EnhancedHardRefresh.Enabled" value="true" />
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.