RX_RMA_TIMES

Field Name

Description

REGION_ID

The ID of the region.

REGION_NAME

The name assigned to the region.

P_MODE

The current prediction mode for the region (e.g., night, default, storm).

MODE_STARTS_UTC

The time that a Prediction mode starts when using Auto Change to set Prediction modes. The value in this table is stored as Coordinated Universal Time (UTC) or Greenwich Mean Time (GMT).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.