Addon Scripts - SQLServer

Addon scripts are available to support optional Responder configurations. By default, these scripts are installed here: \Program Files\Miner and Miner\Responder\Developer Resources\Implementation Scripts\MS-SQL\Addons.

Execute only the scripts for the optional functionality to implement.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.