Report Timeout

For any report run from Archive, you can configure the timeout to be longer. If you do not configure this, the timeout defaults to 30 seconds. However, if you have an abnormally large Archive database, you might want to increase that timeout to allow the reports a little more time to run.

This can be accomplished by adding the following key to the <appSettings> section of Miner.Responder.ArchiveServices.exe.config:

<add key="CommandTimeout" value="<value-in-seconds>" />
TIP: This should only be performed if you have already experienced a report timing out.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.