RX_JUMPERS_HISTORY

Field Name

Description

JUMPER_ID

The ID associated with the Jumper.

JUMPER_FCID

Feature class ID of the Jumper.

JUMPER_OID

The object ID of the Jumper. This field links to the OID field in your geodatabase.

JUMPER_NAME

The name assigned to your Jumper.

TRACE_WEIGHT

Field containing information used by Feeder manager to utilize the Jumper when tracing the network.

WEIGHT_DESC

Description of phases connected by the Jumper.

EDGE_EID1

The edge element ID for the initial click of placing a Jumper.

EDGE_EID2

The edge element ID for the final click of placing a Jumper.

JUNCTION_EID1

The electrical junction to which the initial click of the Jumper is connected.

JUNCTION_EID2

The electrical junction to which the final click of the Jumper is connected.

USER_CREATED

The name of the user who created the jumper. This field is populated automatically by Responder.

USER_UPDATED

The name of the user who updated the jumper. This field is populated automatically by Responder.

FEEDER_ID

All Energized feeders to which either end of a Jumper is connected.

SUBSTATION

The Substations matching the Feeders in FEEDER_ID.

REGION

The region of the initial placement of the jumper.

TIME_OPERATION

Time when the jumper was placed in the field.

TIME_REMOVAL

Time when the jumper was removed in the field.

LOCATION

A text field that can be used to better indicate jumper location.

DISPATCHER

The name of the dispatcher assigned to the jumper. This field is set on the Place Jumper form.

CREW_MEMBER

The name of the crew member assigned to the jumper. This field is set on the Place Jumper form.

COMMENTS

Comments enetered in Responder Explorer for the jumper.

INCIDENT_ID

The ID associated with the incident associated with the jumper. This field acts as a foreign key to the RX_INCIDENTS table.

Points

This field represents all the points on the map a user clicked when creating a Jumper.

CHANGE_DATE

The time and date an operation was performed on the record.

OPERATION

The operation (e.g., insert, delete, update) performed on the record.

JUMPER_GUID

The GUID assigned to the Jumper.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.