RX_INCIDENT_DEVICE_STEPS

Field Name

Description

OPERATION_ID

The ID field from RX_OPERATIONS (foreign key).

EXPECTED_STATUS

The expected or normal status of the device (open, closed).

PLANNED_STATUS

The planned status of the device (e.g, Open, Closed).

PLANNED_CUSTOMER_COUNT

The number of customers affected by a planned step. This value indicates a net change in the number of energized customers. It will be either a positive number (power restored to customers) or negative number (customers losing power).

PLANNED_CRITICAL_COUNT

The number of critical customers affected by a planned step. This value indicates a net change in the number of energized customers. It will be either a positive number (power restored to customers) or negative number (customers losing power).

PLANNED_CONNECTED_LOAD

Amount (in kVA) by which the total system connected load will change due to the planned step.

EXECUTED_CUSTOMER_COUNT

The number of customers affected by an executed step. This value indicates a net change in the number of energized customers. It will be either a positive number (power restored to customers) or negative number (customers losing power).

EXECUTED_CRITICAL_COUNT

The number of critical customers affected by an executed step. This value indicates a net change in the number of energized customers. It will be either a positive number (power restored to customers) or negative number (customers losing power).

EXECUTED_CONNECTED_LOAD

Amount (in kVA) by which the total system connected load will change due to the executed step.

USER_CREATED

The name of the user who created the record. This field is populated automatically by Responder.

USER_UPDATED

The name of the user who updated the record. This field is populated automatically by Responder.

ACTUAL_STATUS

The current actual status of the device (open, closed).

ACTION

The action to be taken by the operation (e.g., open, close).

PHASES

The phase(s) to be operated by the step.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.