RX_T_MAJOR_EVENT_DAY

The Calculate Tmed tool (in Archive Explorer) calculates the Major Event Duration (med) according to the IEEE Standard 1366-2012, section 4.5. When these values are calculated, they are stored in this table. Any incident that has a duration which exceeds the TMED_MINUTES value will be excluded from the Reliability Reports.

Field Name

Description

START_DATE

The outage date (Time of Outage field) of the first load point archive record within the five-year period.

END_DATE

The outage date (Time of Outage field) of the last load point archive record within the five-year period.

TMED_MINUTES

The length of the major event duration (med).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.