Data Services

Data Services is responsible for transferring information input using the web-based call entry form to the Responder database. Use the Data Services tab to configure, manage and execute Data Services. At least one Data Services must be running in order to use the console (i.e., the Count field must contain a value greater than 0). At least one Data Services must be running to access Responder Explorer.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.