Configuration File Updates - 9.2 SP2

This table indicates which Responder configuration files are upgraded for the 9.2 SP2 release. Note that Version Change indicates that only the file-version number has been updated in the configuration file. It is important that this update be made. Upgrades for subsequent releases will fail if the file-version number is not accurate.

TroubleMaker: This application has been extensively enhanced. The 9.2 SP2 installation will overwrite all existing TroubleMaker files. Therefore, no upgrade script is necessary.

  • New: This file is new for this release.

  • Removed: This file does not exist for this release.

  • Upgrade: This file has changed for this release. The existing file must be upgraded.

  • Version Change: This file has not changed for this release. The existing file must be upgraded with file-version number only.

Component

Configuration File

Update

client

Miner.Responder.ArchiveExplorer.exe.config

Version Change

client

Miner.Responder.Explorer.exe.config

Version Change

server

ArchiveQueriesConfig.xml

Upgrade

server

ArchiveSchemaConfig.xml

Upgrade

server

ArchiveStylesConfig.xml

Upgrade

server

ArchiveSubmitRulesConfig.xml

Version Change

server

ControlStylesConfig.xml

Upgrade

server

DataQueriesConfig.xml

Version Change

server

DatabaseSchemaConfig.xml

Upgrade

server

ExplorerRulesConfig.xml

Upgrade

server

Miner.Responder.ArchiveServices.exe.config

Version Change

server

Miner.Responder.DataServices.exe.config

Upgrade

server

Miner.Responder.MessageRouter.exe.config

Version Change

server

Miner.Responder.PredictionServices.exe.config

Upgrade

server

Miner.Responder.WindowsService.exe.config

Version Change

server

SubmitRulesConfig.xml

Upgrade

server

Web.Config**

Upgrade

server

WebRemoting.config**

Version Change

TroubleMaker

Miner.Responder.TroubleMaker.exe.config

New*

web

Web.Config**

Upgrade

web

WebRemoting.config**

Version Change

* Miner.Responder.TroubleMaker.exe.config existed in prior releases. However, drastic enhancements in 9.2 SP1 require that this file be completely overwritten.

**These configuration files exist on both the server and web machines.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.