Customize Symbology in Responder Explorer

Administrators can customize the colors displayed in theResponder Explorer incident grid by editing the controlstylesconfig.xml file on the Responder Server.

To customize the colors, search for <BackColor> and <ForeColor> in the XML file as shown below.

The default colors are listed in Default Symbology in Responder Explorer. Any standard HTML color can be used. Type in a different color name for the incident scenario in the XML file. Visit the W3Schools website for a list of standard HTML color names.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.