Enable Message Queueing

Client machines, Responder services, and the web server must have Message Queueing enabled. If you are hosting multiple Responder components on a single machine (e.g., Responder services and web server), this step needs to be performed only once. For Responder Services, you must assign permissions to the Oracle directory.

Windows 8 & 10

  1. From the Windows Control Panel, select Programs.
  2. Select Turn Windows features on or off.
  3. Expand Microsoft Message Queue (MSMQ) Server.
  4. Check the Multicasting Support checkbox. This is the minimum requirement for Responder.
    NOTE: If selected, we recommend clearing the MSMQ Active Directory Domain Services Integration option unless it is absolutely necessary for other product's functionality.
  5. Click OK.

Windows 7

  1. From the Windows Control Panel, select Programs.
  2. Select Turn Windows features on or off.
  3. Expand Microsoft Message Queue (MSMQ) Server.
  4. Check the Multicasting Support checkbox. This is the minimum requirement for Responder.
    NOTE: If selected, we recommend clearing the MSMQ Active Directory Domain Services Integration option unless it is absolutely necessary for other product's functionality.
  5. Click OK.

Windows Server 2016

  1. Open Server Manager.
  2. In the Dashboard click Add Roles and Features.
  3. In the Add Roles and Features Wizard, select Role-based or Feature-based installation and click Next.
  4. Select a server from the server pool and click Next.
  5. Click Next in Server Roles.
  6. Under Features, expand Message Queuing.
  7. Check the boxes for Message Queuing Server and for Multicasting Support.
  8. Click Next.
  9. Click Install.

Windows Server 2012

  1. Open Server Manager.
  2. In the Dashboard click Add Roles and Features.
  3. In the Add Roles and Features Wizard, select Role-based or Feature-based installation and click Next.
  4. Select a server from the server pool and click Next.
  5. Click Next in Server Roles.
  6. Under Features, expand Message Queuing.
  7. Check the boxes for Message Queuing Server and for Multicasting Support.
  8. Click Next.
  9. Click Install.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.