RX_HAZARDS_HISTORY

Field Name

Description

HAZARD_ID

The ID associated with the hazard. This field acts as a foreign key to the RX_HAZARDS table.

INCIDENT_ID

The ID associated with the incident. This field acts as a foreign key to the RX_INCIDENTS table.

CALL_ID

The unique identifier associated with the call. This field corresponds with the ID field in the RX_CALLS table.

FCID

Feature class ID of the feature associated with the tag.

OID

Object ID of the feature associated with the tag.

SUBID

The unique ID of each segment of a complex edge.

FACILITY_ID

The Facility ID of the incident device as defined in the geodatabase.

X

The x-coordinate of the incident device.

Y

The y-coordinate of the incident device.

DAMAGE_TYPE

This is the hazard type. This field uses the HAZARD_TYPE domain.

STATUS

Indicates the status of the hazard. This field uses the STATUS domain.

WIRE_OWNER

The owner of the "wires down" hazard. This field uses the HAZARD_TYPE_OWNER domain.

TIME_CREATED

The time the hazard incident was created.

TIME_COMPLETED

Indicates the time that the hazard was fixed.

TIME_SECURED

Indicates the time that the hazard was made secure.

TIME_PUBLIC_SAFETY_ARR

The time a public safety official arrived at the hazard scene.

TIME_PUBLIC_SAFETY_REL

The time a public safety official was relieved from the hazard scene.

REMARKS

Notes from the operator or dispatcher.

USER_CREATED

The name of the user who created the record. This field is populated automatically by Responder.

USER_UPDATED

The name of the user who updated the record. This field is populated automatically by Responder.

CANCEL_REASON

Reason the hazard was cancelled.

CHANGE_DATE

The time and date an operation was performed on the callback record.

OPERATION

The operation (e.g., insert, delete, update) performed on the incident device.

ADDRESS

The address where the incident is located

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.