RX_INCIDENT_FEATURES_HISTORY

Much of the data in this table may be viewed on the Responder Explorer Incidents tab by right-clicking a location feature and selecting Edit.

Field Name

Description

INCIDENT_FEATURE_ID

The unique identifier assigned to the incident feature. This field corresponds to the ID field in the RX_INCIDENT_FEATURES table.

OID

Object ID of the feature associated with the incident.

FCID

Feature class ID of the feature associated with the incident.

SUBID

The unique ID of each segment of a complex edge.

X

The x-coordinate of the incident feature.

Y

The y-coordinate of the incident feature.

INCIDENT_ID

The ID associated with the incident. This field corresponds with the ID field in the RX_INCIDENTS table.

TIME_REPORTED

Time that the feature was reported out.

CONFIRMED

Indicates whether the feature has been confirmed out. This field uses the CONFIRMED domain.

FACILITY_ID

The Facility ID of the incident feature as defined in the geodatabase.

USER_CREATED

This field is not currently used by Responder. You may customize Responder to populate this field with the name of the user who created the record.

USER_UPDATED

This field is not currently used by Responder. You may customize Responder to populate this field with the name of the user who updated the record.

REMARKS

Notes from the operator or dispatcher.

CHANGE_DATE

The date an operation was performed on the incident record.

OPERATION

The operation (e.g., insert, delete, update) performed on the incident record.

CANCEL_REASON

Reason the feature was cancelled.

ADDRESS

The address where the incident is located

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.