RX_SWITCHING_ORDERS

Field Name

Description

NAME

The user-defined name of the switching order.

INCIDENT_ID

The ID of the incident associated with the switching order.

TYPE

Indicates a switching order or a restoration plan.

TIME_BEGIN

Start time for the switching order.

TIME_END

Finish time for the switching order.

REQUESTED_BY

Name of the person who requested the switching order.

TIME_REQUESTED

The time the switching order was requested.

CREATED_BY

The user name of the person who created the switching order.

TIME_CREATED

The time the switching order was created.

APPROVED_BY

User name of the person who approved the switching order.

TIME_APPROVED

The time that the switching order was approved.

REMARKS

Remarks associated with the switching order.

USER_CREATED

The name of the user who created the record. This field is populated automatically by Responder.

USER_UPDATED

The name of the user who updated the record. This field is populated automatically by Responder.

REGION

The region in which the incident resides.

STATUS

Indicates the status of the switching order. This field uses the STATUS domain.

FOLDER_ID

ID of the Switching Order Library folder in which the switching order resides. This field corresponds to the ID field in the SWITCHING_ORDER_FOLDERS table.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.