RX_CREW_ASSIGNMENTS_ARCHIVE

Field Name

Description

ASSIGNMENT_ID

The unique identifier assigned to each crew assignment. This field corresponds with the ID field in the RX_CREW_ASSIGNMENTS table.

INCIDENT_ID

The ID associated with the incident. This field corresponds with the ID field in the RX_INCIDENTS table.

CREW_ID

Indicates the ID for the crew that has been assigned to the incident. This field corresponds to the ID field in the RX_CREWS table.

STATUS

Indicates the status of the crew. This field uses the STATUS domain.

TIME ASSIGNED

The time the crew was assigned to the incident.

IS_LEAD_CREW

Indicates whether the crew is the lead crew. This field uses the IS_LEAD_CREW domain.

USER_CREATED

The name of the user who created the record. This field is populated automatically by Responder.

USER_UPDATED

The name of the user who updated the record. This field is populated automatically by Responder.

CHANGE_DATE

The time and date an operation was performed on the record.

OPERATION

The operation (e.g., insert, delete, update) performed on the record.

USER_UPDATED_ARCH

This field is not currently used by Responder. You may customize Responder to populate this field with the name of the user who updated the record.

TIME_STATUS_CHANGED

This is the time that a crew's status was changed (e.g., from Dispatched to Working) after it was modified by a dispatcher.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.