Creating the Abnormal Line Display Layer

NOTE: This is optional. Abnormal is needed as a separate layer only if you require specific labeling or display needs that cannot be done using one layer with de-energized and abnormal lines. See the Creating the De-energized Line Display Layer section above to create one layer with both de-energized and abnormal lines.
  1. Add the RxLineDisplay layer to the Responder_Cached group in your map.
  2. Right-click RxLineDisplay and select Properties.
  3. Select the Symbology tab.
  4. Type Abnormal in the Label appearing next to the symbol in the Table of Contents field.
  5. Click the line symbol to modify the color and size used to display it on the map.
  6. Select the Definition Query tab.
  7. Enter the following in the Definition Query field: RXFEEDERID not like ('%,%') or RXFEEDERID is not null (using the field that is assigned the RXFEEDERID model name).
  8. Click OK to save changes in the Layer Properties.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.