RX_SWITCHING_ORDERS_ARCHIVE

Field Name

Description

ORDER_ID

The ID associated with a switching order. This field corresponds to the ID field in the RX_SWITCHING_ORDERS table.

NAME

The name of the switching order.

INCIDENT_ID

The ID associated with the incident. This field corresponds with the ID field in the RX_INCIDENTS table.

TYPE

Indicates the type of operation (custom, tag, or device).

REGION

The region in which the incident is located. This field uses the REGION domain.

TIME_BEGIN

Start time for the switching order.

TIME_END

Finish time for the switching order.

REQUESTED_BY

Name of the person who requested the switching order.

TIME_REQUESTED

The time the switching order was requested.

TIME_CREATED

The time the switching order was created.

APPROVED_BY

User name of the person who approved the switching order.

STATUS

Indicates the status of the switching order. This field uses the STATUS domain.

REMARKS

Remarks associated with the switching order.

USER_CREATED

The name of the user who created the record. This field is populated automatically by Responder.

USER_UPDATED

The name of the user who updated the record. This field is populated automatically by Responder.

CHANGE_DATE

The time and date an operation was performed on the record.

OPERATION

The operation (e.g., insert, delete, update) performed on the record.

USER_UPDATED_ARCH

This field is not currently used by Responder. You may customize Responder to populate this field with the name of the user who updated the record.

CREATED_BY

The user name of the person who created the switching order.

TIME_APPROVED

The time that the switching order was approved.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.