Description

You can change the description of a Responder Archive Explorer report by editing the Value attribute of the report's Description property.

To change the description that appears when selecting a report in Archive Explorer:

  1. Open ArchiveQueriesConfig.xml. By default, this file is installed here: C:\Program Files (x86)\Miner and Miner\Responder\Server.
  2. Look for the following XML.
    <QueryClass Key="IncidentID" Caption="Incident by ID" Category="Browser">
              <Properties>
                <b:Property Key="Description" Value="A detailed report of the incident for an incident ID." /> 
    TIP: Making changes to any Archive Explorer report that has a QueryClass Category="Browser" will modify that same report in Responder Web.

    The above XML indicates the description that is visible for the Incident by ID report. By default, each report has a description.

  3. Search for the appropriate report to edit the description. Report names are found in the Caption attribute. 
    TIP: Each report appears twice in ArchiveQueriesConfig.xml - once for the Category of Browser and once for Excel.
  4. Replace the Value attribute of the description with the appropriate text.
  5. Repeat these steps for the same report with a Category attribute of Excel.
  6. Save and close ArchiveQueriesConfig.xml. There is no need to edit ArchiveSchemaConfig.xml for this configuration.
  7. Close and reopen Responder Archive Explorer to view the updated changes.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.